1 of 1(100%)customers would recommend this product to a friend.
Customer Reviews for APC Smart-UPS XL Modular 3000VA 120V Rackmount/Tower
Review 1 for APC Smart-UPS XL Modular 3000VA 120V Rackmount/Tower
Overall:
5out of5
Reviewed by: John
Location:New York, NY
Customer Type:Large Corporation (more than 1000 employees)
Role:General IT Management
Product application:Datacenter & IT Infrastructure: Racks and Accessories
I've used this product(s) for:over 5 years
Title: More then enough
Date:August 22, 2010
"I started a position as an IT manager and one of the things that needed to be done was enclose all the servers in a rack. Well i needed to choose one UPS to provide battery backup to these 7 servers. I chose this to test and it is more than what i expected. I have seven servers, a 24 port gigabit switch, a kvm box and a slide out monitor and keyboard plugged into it and only 2 of the load lights are on. We had a power outage and this baby lasted over 20 minutes!!!! Really great UPS or the money and size and overall ease. Network Management card is great. Sends automated emails and provides SNMP Monitoring."